Code banking.exe is a command line utility. Navigate to the path of the host application through command prompt and use the command line

code banking.exe firmwarename.hex

Here firmwarename is the name of the output firmware hex file of the code banked firmware.

Note:- 
1. Code banker.hex is used during firmware download process and has to be present in the same folder as code banking.exe.
2. During firmware download the device renumerates many times based on the number of code banks used. 
3. This source is generic and with information on the code bank memory location parameters it can be optimized.